/content/hbtbt/us/en/search-results.html
    IMPORTANT: You are Viewing Ring-Fenced Materials. DO NOT share this content via email, screen shots or messages with anyone else.

    Port Esbjerg Deploys Honeywell Solution To Help Meet 70% Carbon Reduction Target

     

     

    ·         Extensive carbon and energy management initiative introduces shore-to-ship power units

    ·         Further carbon emissions reduction plans already in place to meet sustainability goals

    In a global first for the maritime industry, Port Esbjerg and Honeywell are working together on a climate co-operation designed to help reduce carbon emissions at the Danish port by 70% by 2030 in line with the country’s climate target.

    Port Esbjerg, located on the south-west coast of Denmark, is working with Honeywell on a comprehensive carbon and energy management programme to help achieve the port’s emissions reduction goal. The initiatives also contribute towards the International Maritime Organization’s ambition to halve greenhouse gases from international shipping by 2050, compared with 2008 levels

    The Port Esbjerg team recently inaugurated its first shore-to-ship power units, which allow docked vessels to run on renewable electricity from offshore wind turbines, instead of using on-board diesel generators.

    This power connection is enabled by the cooperation between Honeywell and Port Esbjerg, specifically supported through understanding estimations of the vessels’ carbon footprint. The port can access this data at any time through the Honeywell Enacto Carbon and Energy Management system. The shore-to-ship units can simultaneously power multiple large vessels, helping to reduce CO2, SOx and NOx emissions, as well as reducing noise pollution.

    “Given the size and complexity of our operation, there was no simple, off-the-shelf solution for our green transition. We worked with Honeywell to fully customise a system that can monitor energy consumption and emissions, as well as pinpoint potential improvement opportunities,” explains Port Esbjerg CEO, Dennis Jul Pedersen.

    The Honeywell Enacto Carbon and Energy Management system is a cloud-based, fully scalable solution that enables the port to monitor the emissions and resource consumption of every individual power socket, and – most importantly – every vessel, with 1,200 measurement points. The system uses artificial intelligence and machine learning algorithms in conjunction with data collection from energy-consuming or -producing assets at the port. Its open protocol platform allows for flexible and seamless integration with legacy systems.

    If consumption changes significantly, the system sends an automated message to the port office, meaning any abnormalities are immediately identified and action may be taken. Vessels’ carbon emissions are closely observed with the aim of reduction through operational investments in sustainable infrastructure, including use of renewable energy, and in the future - clean fuel technology.

    Based on data generated by the Honeywell system, Port Esbjerg can optimise its energy and carbon footprint in real time. In the future, it will be able to prioritise financial resources where the most significant CO2 reductions can be made – generating tangible emissions-lowering results.

    “The Port Esbjerg project is setting a new benchmark for ports globally on how to use fully integrated technology to help meet ambitious sustainability goals,” says Lionel Caillat, General Manager, Honeywell Building Technologies. “We worked closely with the Port Esbjerg team to understand their objectives and customise a solution that can help to achieve them. It’s exciting to go from initial planning to seeing the port meet their renewable shore-to-ship power supply milestone. We look forward to our continued work with the port to help them cut emissions down further.”

    In the next phase of the project, Port Esbjerg and Honeywell will monitor and manage water consumption and heating, as well as the emissions performance of businesses around the port. The plan also features significant investments in electric vehicle technology and hydrogen-powered cranes. The target is for all port vehicles to be powered by electricity by 2025.

    About Honeywell Building Technologies

    Honeywell Building Technologies (HBT) is transforming the way every building operates to help improve the quality of life. We are a leading building controls company with operations in more than 75 countries supported by a global channel partner network. Commercial building owners and operators use our hardware, software and analytics to help create safe, efficient and productive facilities. Our solutions and services are used in more than 10 million buildings worldwide.

    Honeywell (www.honeywell.com) is a Fortune 100 technology company that delivers industry specific solutions that include aerospace products and services; control technologies for buildings and industry; and performance materials globally. Our technologies help aircraft, buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/newsroom. 

    About Port Esbjerg

    Port Esbjerg is one of the largest ports in Denmark and is one of the primary ports in Europe for shipping and installation of offshore wind, but is also the key port for the Danish oil and gas operations, while also the farming and fishing industries use this port heavily for export and imports. The Port of Esbjerg is the European market leader when it comes to handling and shipping out wind power. More than 4/5 of the offshore wind capacity installed in Europe was shipped out from the port. There are more than one hundred companies operating within the port and they employ nearly 17,000 people.
    For more news and information, please visit Port Esbjerg

    Megan McGovern
    Honeywell Building Technologies
    Alex Smith
    Weber Shandwick